POWER OF ATTORNEY
Know all by these presents, that the undersigned hereby constitutes and appoints each of Joseph R.
Leonti, Kristen L. Gest, and Kelley B. Standard, or any of them signing singly, and with full power of
substitution, the undersigned's true and lawful attorney-in-fact to:
(1) prepare, execute in the undersigned?s name and on the undersigned?s behalf, and submit
to the U.S. Securities and Exchange Commission (the ?SEC?) a Form ID, including
amendments thereto, and any other documents necessary or appropriate to obtain codes
and passwords enabling the undersigned to make electronic filings with the SEC of reports
required by Section 16(a) of the Securities Exchange Act of 1934 or any rule or regulation
of the SEC;
(2) execute for and on behalf of the undersigned, in the undersigned's capacity as an officer
and/or director of Parker-Hannifin Corporation (the ?Company?), Forms 3, 4, and 5 in
accordance with Section 16(a) of the Securities Exchange Act of 1934 and the rules
thereunder;
(3) do and perform any and all acts for and on behalf of the undersigned which may be
necessary or desirable to complete and execute any such Form 3, 4, or 5, complete and
execute any amendment or amendments thereto, and timely file such form with the SEC
and any stock exchange or similar authority; and
(4) take any other action of any type whatsoever in connection with the foregoing which, in the
opinion of such attorney-in-fact, may be of benefit to, in the best interest of, or legally
required by, the undersigned, it being understood that the documents executed by such
attorney-in-fact on behalf of the undersigned pursuant to this Power of Attorney shall be in
such form and shall contain such terms and conditions as such attorney-in-fact may
approve in such attorney-in-fact's discretion.
The undersigned hereby grants to each such attorney-in-fact full power and authority to do and
perform any and every act and thing whatsoever requisite, necessary, or proper to be done in the exercise
of any of the rights and powers herein granted, as fully to all intents and purposes as the undersigned might
or could do if personally present, with full power of substitution or revocation, hereby ratifying and
confirming all that such attorney-in-fact, or such attorney-in-fact's substitute or substitutes, shall lawfully do
or cause to be done by virtue of this power of attorney and the rights and powers herein granted. The
undersigned acknowledges that the foregoing attorneys-in-fact, in serving in such capacity at the request of
the undersigned, are not assuming, nor is the Company assuming, any of the undersigned's responsibilities
to comply with Section 16 of the Securities Exchange Act of 1934.
This Power of Attorney shall remain in full force and effect until the undersigned is no longer
required to file Forms 3, 4, and 5 with respect to the undersigned's holdings of and transactions in
securities issued by the Company, unless earlier revoked by the undersigned in a signed writing delivered to
the foregoing attorneys-in-fact.
IN WITNESS WHEREOF, the undersigned has caused this Power of Attorney to be executed as of
this 15th day of August, 2017.
/s/ Martin C. Maxwell
Martin C. Maxwell
\\\DC - 57385/2 - #1301253 v1
\\\DC - 57385/2 - #1301253 v1