« Back

Parker Hannifin Releases Revolutionary Oil Production System

May 18, 2009

OIL CITY, La., May 18 /PRNewswire-FirstCall/ -- Angel Petroleum Technologies, LLC., announces that the BlackStorm Oil Production System (BPS) has been released to market under license to Parker Hannifin Corp. (NYSE: PH). The BPS replaces rods, tubing, beam pump, polish rod, workover rig and eliminates treatments for tubing corrosion.

The BPS is a revolutionary corrosion-proof, one piece oil production system combining the durability of a purpose-built thermoplastic tubing system with the efficiency of an Electric Submersible Pump (ESP). The ESP power cable and a stainless steel wire rope are integrated into the tubing string allowing one man installation without a workover rig.

Labor cost for a typical equipment relocation drops by more than 95% with much lower Worker's Compensation rates due to enhanced safety. Turnkey installation time from drive up to drive away is less than 20 minutes. The BPS is projected to pay for itself in less than 3 years on the basis of reduced maintenance, elimination of workover rig and no chemical treatments required for corrosion. Fluid moving costs are typically over 50% less than with a traditional beam pump.

BlackStorm is manufactured by the ParFlex Division of Parker Hannifin under royalty bearing license from Angel Petroleum Technologies, LLC. Protected distribution areas for the BPS are available.

About Angel Petroleum Technologies, LLC.:

Angel Petroleum is a privately held company focused on the development of novel, cost-effective solutions for the stripper well industry. Other technologies under development include oil/water separation systems (OWS) and small-scale enhanced oil recovery (EOR) technologies. Source: Angel Petroleum Technologies, LLC.

For more information contact: Jay Reynolds at (318) 208-1137
jayreynolds@wb4me.com
www.blackstormsystem.com

About Parker Hannifin:

With annual sales exceeding US$10 billion, Parker Hannifin is the world's leading diversified manufacturer of motion and control technologies and systems, providing precision-engineered solutions for a wide variety of commercial, mobile, industrial, and aerospace markets. The company employs more than 57,000 people in 43 countries around the world. Parker has increased its annual dividends paid to shareholders for 51 consecutive years, among the top five longest-running dividend-increase records in the S&P 500 index. For more information, visit the company's web site at http://www.parker.com, or its investor information site at http://www.phstock.com. SOURCE Parker Hannifin Corporation

SOURCE Angel Petroleum Technologies, LLC.; Parker Hannifin Corporation

CONTACT:
Jay Reynolds, +1-318-208-1137
jayreynolds@wb4me.com
for Angel Petroleum Technologies, LLC.
and Parker Hannifin Corporation

/Web Site: http://www.parker.com http://www.phstock.com http://www.blackstormsystem.com

Angel Petroleum Technologies, LLC.; Parker Hannifin Corporation ST: Louisiana IN: OIL GAS UTI MAC SU: PDT LIC PR -- DA18924 -- 6024 05/18/200916:51 EDThttp://www.prnewswire.com -->

Follow Us

Follow Parker Hannifin on social media:
Follow Parker Hannifin on social media